Custom training¶
Overview¶
On our Github repo depthai-ml-training we provide several ML training notebooks trained on various data sets. You can run these notebooks on Google Colab - they provide free CPU/GPU instances, so great for prototyping and even simple production models.
We currently have these ML training tutorials:
The Tutorials¶
Easy Object Detector Training 
The tutorial notebook Easy_Object_Detection_With_Custom_Data_Demo_Training.ipynb shows how to quickly train an object detector based on the MobileNet SSDv2 network.
Optionally, see our documentation around this module (here) for of a guide/walk-through on how to use this notebook. Also, feel free to jump right into the Notebook, with some experimentation it’s relatively straightforward to get a model trained.
After training is complete, it also converts the model to a .blob file that runs on our DepthAI platform and modules. First the model is converted to a format usable by OpenVINO called Intermediate Representation, or IR. The IR model is then compiled to a .blob file using a server we set up for that purpose. (The IR model can also be converted locally to a blob.)
And that’s it, in less than a couple of hours a fairly advanced proof of concept object detector can run on DepthAI to detect objects of your choice and their associated spatial information (i.e. X, Y, Z coordinates). For example this notebook was used to train DepthAI to locate strawberries in 3D space, see below:
COVID-19 Mask/No-Mask Training 
The Medical Mask Detection Demo Training.ipynb training notebook shows another example of a more complex object detector. The training data set consists of people wearing or not wearing masks for viral protection. There are almost 700 pictures with approximately 3600 bounding box annotations. The images are complex: they vary quite a lot in scale and composition. Nonetheless, the object detector does quite a good job with this relatively small data set for such a task. Again, training takes around 2 hours. Depending on which GPU the Colab lottery assigns to the notebook instance, training 10k steps can take 2.5 hours or 1.5 hours. Either way, a short period for such a good quality proof of concept for such a difficult task. We then performed the steps above for converting to blob and then running it on our DepthAI module.
Supporting Notebooks¶
Image Resize in Google Drive 
This notebook operates on your set of images in Google Drive to resize them to the format needed by the training notebooks.