Troubleshooting¶
DepthAI can’t connect to an OAK camera¶
For USB OAK cameras, DepthAI can throw an error code like X_LINK_COMMUNICATION_NOT_OPEN or X_LINK_ERROR,
which is usually a sign of a bad USB3 cable (or a USB2 cable). If you are using USB2 cable (and want USB2 bandwidth),
you have to specify USB2 protocol, see Forcing USB2 Communication for more information. Another common
issue is that users haven’t set udev rules on their Linux machine.
If you still can’t connect to the OAK camera, you should execute lsusb | grep 03e7. You should see a similar line:
$ lsusb | grep 03e7
Bus 001 Device 120: ID 03e7:2485 Intel Movidius MyriadX
Another thing to check is the dmesg -w. After executing that and pressing enter a few times (for separator), connect
your OAK camera to the host. You should see a similar output in the terminal:
/~$ dmesg -w
[223940.862544] usb 1-3.2: new high-speed USB device number 120 using xhci_hcd
[223940.963357] usb 1-3.2: New USB device found, idVendor=03e7, idProduct=2485, bcdDevice= 0.01
[223940.963364] usb 1-3.2: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[223940.963368] usb 1-3.2: Product: Movidius MyriadX
[223940.963371] usb 1-3.2: Manufacturer: Movidius Ltd.
[223940.963373] usb 1-3.2: SerialNumber: 03e72485
For PoE OAK cameras, see PoE Troubleshooting page.
If these commands didn’t return the expected log, see Support page.
Reporting firmware crash dump¶
Steps to create a crash dump:
Run a code that causes the firmware crash
Afterwards, please send the generated .txt file to us (email/github/forum), and our development team will try to fix the cause of the crash as soon as possible.
Ping was missed, closing the device connection¶
[host] [warning] Monitor thread (device: 194435108198757340 [169.254.1.222]) - ping was missed, closing the device connection
This error is mostly seen on POE cameras, and can sometimes occur after a few hours or even days of running the pipeline. It happens because device doesn’t reply to ping messages, which usually happens if device is too busy (high CPU consumption), or there’s a networking issue. Potential solutions include:
Lower OAK CPU consumption
If CPU usage is above 95% that can be a bad sign. You can measure CPU usage by running the depthai in debug mode. A few options to reduce CPU consumption are:
Update networking settings on host computer - using
ethtool, some have reported that increasingrx-usecsfrom 0 to 400 decreased Leon CPU usage from 99% to 93%Reducing the pipeline / resolution / FPS, so there’s less computation happening on the camera
Increasing watchdog timeout
Another solution is to increase watchdog timeout, so it isn’t as “trigger happy”. Default value for POE devices is 4000 ms, and user can set it to 4500ms (max value). This can be done by setting environmental variable
DEPTHAI_WATCHDOG, so for example on linux:DEPTHAI_WATCHDOG=4500 python3 my_app.py.
Implementing re-connection
This would be quite recommended, as it would allow the application to recover from the error. So whenever there’s an error, re-connect to the device and continue running the pipeline.
For depthai API, this could be implemented as:
pipeline = dai.Pipeline()
# ...
while True:
# Every time it crashes, re-initialize the device and upload the pipeline to it
with dai.Device(pipeline) as device:
queue = device.getOutputQueue("name")
while True:
q.get()
Standalone mode
If you run your device in Standalone mode and communicate with it via networking protocols (TCP/UDP/HTTP/MQTT) and not XLink, there’s no ping mechanism, so this error won’t occur. If there were an issue on device side (which is why we have watchdog in the first place), device would auto-restart.
ImportError: No module named ‘depthai’¶
This indicates that the depthai was not found by your python interpreter. There are a handful of reasons this can fail:
Is the Python API installed? Verify that it appears when you type:
python3 -m pip list | grep depthai
Are you using a supported platform for your operating system? If not, you can always install from source:
cat /etc/os-release
Why is the Camera Calibration running slow?¶
Poor photo conditions can dramatically impact the image processing time) during the camera calibration. Under normal conditions, it should take 1 second or less to find the chessboard corners per-image on an Raspberry Pi but this exceed 20 seconds per-image in poor conditions. Tips on setting up proper photo conditions:
Ensure the checkerboard is not warped and is truly a flat surface. A high-quality option: print the checkerboard on a foam board.
Reduce glare on the checkerboard (for example, ensure there are no light sources close to the board like a desk lamp).
Reduce the amount of motion blur by trying to hold the checkerboard as still as possible.
Permission denied error¶
If python3 -m pip install fails with a Permission denied error, your user likely doesn’t have permission
to install packages in the system-wide path.
[Errno 13] Permission denied: '/usr/local/lib/python3.7/dist-packages/...'
Try installing in your user’s home directory instead by adding the --user option. For example:
python3 -m pip install depthai --user
DepthAI does not show up under /dev/video* like web cameras do. Why?¶
The USB device enumeration could be checked with lsusb | grep 03e7 . It should print:
03e7:2485after reset (boot loader running)03e7:f63bafter the application was loaded
No /dev/video* nodes are created. See OAK as a webcam if you would like to use OAK camera as a webcam.
Intermittent Connectivity with Long (2 meter) USB3 Cables¶
We’ve found that some hosts have trouble with long USB3 cables (above 6ft/2m). It seems to have something to do with the USB controller on the host side. For example, all Apple computers we’ve tested with have never exhibited the problem, as Apple computers have powerful USB controllers.
So, if you experience this problem with your host, there are potentially 3 options:
Switching to a shorter USB3 cable (say 1 meter) will very likely make the problem disappear. These 1 meter (3.3 ft.) cables are a nice length and are shipped with OAK USB3 variants.
Force USB2 mode. This will allow use of the long cable still, and many DepthAI use cases do not necessitate USB3 communication bandwidth - USB2 is plenty.
Use Active USB3 cable. We have tested this 10m active cable and USB3 works as expected (even without powering the repeater).
Note that Ubuntu 16.04 has an independent USB3 issue, seemingly only on new machines though. We think this has to do w/ Ubuntu 16.04 being EOLed prior to or around when these new machines hit the market. For example, this computer (here) has rampant USB3 disconnect issues under Ubuntu 16.04 (with a 1 meter cable), but has none under Ubuntu 18.04 (with a 1 meter cable).
Forcing USB2 Communication¶
If you aren’t using a (working) USB3 cable or your host computer doesn’t support USB3, you should force the USB2 communication. It’s also recommended to use USB2 communication if you are using a longer USB cable (2m+).
For API usage, set the maxUsbSpeed=dai.UsbSpeed.HIGH when creating the dai.Device object
# Force USB2 communication
with dai.Device(pipeline, maxUsbSpeed=dai.UsbSpeed.HIGH) as device:
# ...
If you are using depthai_demo you can specify USB speed
with -usbs argument:
python3 depthai_demo.py -usbs usb2
Output from DepthAI keeps freezing¶
If the output from the device keeps freezing every few seconds, there may be a problem with the USB3 connection and forcing the device into USB2 mode could resolve this issue - instructions are in the chapter above.
When connection speed is USB2 (due to some hosts - Windows in particular - or USB controller/port/cable being USB2) - initialization of USB3-enabled firmware or streaming after a few frames may fail. The workaround here is to force the device to use the USB2-only firmware (mentioned in the chapter above).
DepthAI freezes after a few frames¶
If your app freezes and you don’t get any new messages from the device after a few messages (eg. 4 frames) after booting, it’s likely that queues filled up and were set to blocking mode. Additional details on node queues (on the OAK device) can be found here. We also recommend using Pipeline Graph tool to quikcly check if there is something wrong with the pipeline (eg. a node that isn’t connected to anything).
Udev rules on Linux¶
Failed to boot the device: 1.3-ma2480, err code 3Failed to find device (ma2480), error message: X_LINK_DEVICE_NOT_FOUND[warning] skipping X_LINK_UNBOOTED device having name "<error>"Insufficient permissions to communicate with X_LINK_UNBOOTED device with name "1.1". Make sure udev rules are set
If you are getting any of the errors above, it’s most likely that udev rules are not set on your Linux machine.
To fix this, set the udev rules using the commands below, unplugging DepthAI and then plugging it back into USB afterwards.
echo 'SUBSYSTEM=="usb", ATTRS{idVendor}=="03e7", MODE="0666"' | sudo tee /etc/udev/rules.d/80-movidius.rules
sudo udevadm control --reload-rules && sudo udevadm trigger
CTRL-C Is Not Stopping It!¶
If you are trying to kill a program with CTLR-C, and it’s not working, try CTRL-\ instead. Usually this will work.
Nothing happening when running a DepthAI script¶
If upon running a DepthAI script, nothing happens (the script just hangs) and you cannot CTRL-C out of it.
Try running cam_test.py script from the depthai-python/utilities folder. The script should error out with something like:
QObject::moveToThread: Current thread (0x55b9d0a00320) is not the object's thread (0x55b9d0cad7e0).
Cannot move to target thread (0x55b9d0a00320)
.
.
.
Aborted (Signal sent by tkill() 32104 1001)
Aborted (core dumped)
This means there is a problem with PyQt5 installation. Follow this issue for a resolution.
“DLL load failed while importing cv2” on Windows¶
If you are seeing the following error after installing DepthAI for Windows:
(venv) C:\Users\Context\depthai>python depthai_demo.py
Traceback (most recent call last):
File "C:\Users\Context\depthai\depthai_demo.py", line 7, in <module>
import cv2
File "C:\Users\Context\depthai\venv\lib\site-packages\cv2\__init__.py", line 5, in <module>
from .cv2 import *
ImportError: DLL load failed while importing cv2: The specified module could not be found.
Then installing the Windows Media Feature Pack (here) is often the resolution, as Media Feature Pack must be installed for Windows 10 N editions.
(And more background from OpenCV directly is here)
python3 depthai_demo.py returns Illegal instruction¶
This so far has always meant there is a problem with the OpenCV install on the host (and not actually with the depthai library). To check this, run:
python3 -c "import cv2; import numpy as np; blank_image = np.zeros((500,500,3), np.uint8); cv2.imshow('s', blank_image); cv2.waitKey(0)"
If a window is not displayed, or if you get the Illegal instruction result, this means there is a problem with
the OpenCV install. The installation scripts here
often will fix the OpenCV issues. But if they do not, running
python3 -m pip install opencv-python --force-reinstall
will often fix the OpenCV problem.
Neural network blob compiled with incompatible openvino version¶
[NeuralNetwork(2)] [error] Neural network blob compiled with incompatible openvino version. Selected openvino version 2020.3. If you want to select an explicit openvino version use: setOpenVINOVersion while creating pipeline
The reason for this error is that depthai can’t resolve the OpenVINO version from the blob. The solution is simple, the user has to specify the OpenVINO version with which the blob was compiled (as mentioned in the error message):
pipeline = depthai.Pipeline()
# Set the correct version:
pipeline.setOpenVINOVersion(depthai.OpenVINO.Version.VERSION_2021_1)
“realloc(): invalid pointern Aborted” on RPi¶
On RPi, after running sudo apt upgrade, you might get the error realloc(): invalid pointer\n Aborted when importing cv2 after depthai library. We have observed the same issue, and have found a solution:
Downgrade libc6 by running
sudo apt install -y --allow-downgrades libc6=2.28-10+rpi1, ORRe-install DepthAI dependencies by running
sudo curl -fL http://docs.luxonis.com/_static/install_dependencies.sh | bash
[error] Attempted to start camera - NOT detected!¶
If you are facing any of the errors above for either Mono Left/Right or Color camera, first try using the latest depthai version (python3 -mpip install depthai -U).
If that doesn’t help, there are 2 probable causes:
You are using OAK FFC and a camera sensor that isn’t supported by default, so you should use a different branch, see docs here.
A camera got disconnected during the shipping. This has been reported only a handful of times, but it’s possible.
The solution here is to open up the enclosure and re-attach the connector to the camera, see the image here for the OAK-D (left mono camera not detected).
[error] input tensor exceeds available data range¶
[NeuralNetwork(3)] [error] Input tensor '0' (0) exceeds available data range. Data size (6336B), tensor offset (0), size (6912B) - skipping inference
This error is usually thrown when we use NNData message and we don’t provide the amount of bytes that the NN model
expects for the inference. For example, in the error above, the NN model expects 6912 bytes (48x48x3), but only 6336 bytes
were sent to it.
Converting YUV420 to CV2 frame¶
If you try to convert YUV420 frame to CV using ImgFrame’s .getCvFrame()
method, you might come accross the error below:
cv2.error: OpenCV(4.6.0) d:\a\opencv-python\opencv-python\opencv\modules\imgproc\src\color.simd_helpers.hpp:108: error:
(-215:Assertion failed) sz.width % 2 == 0 && sz.height % 3 == 0 in function
'cv::impl::`anonymous-namespace'::CvtHelper<struct cv::impl::`anonymous namespace'::Set<1,-1,-1>,
struct cv::impl::A0xe823dd8f::Set<3,4,-1>,struct cv::impl::A0xe823dd8f::Set<0,-1,-1>,1>::CvtHelper'
The culprit of the error is that OpenCV requires YUV420 width to be divisible by 2, and height to be divisible by 3. A simple example that will crash:
1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 | import depthai as dai import cv2 pipeline = dai.Pipeline() cam = pipeline.createColorCamera() manip = pipeline.createImageManip() # manip.initialConfig.setFrameType(dai.RawImgFrame.Type.BGR888p) manip.initialConfig.setResize(600, 451) cam.isp.link(manip.inputImage) xout = pipeline.createXLinkOut() xout.setStreamName("out") manip.out.link(xout.input) with dai.Device(pipeline) as device: f = device.getOutputQueue('out').get().getCvFrame() cv2.imshow("frame", f) cv2.waitKey(0) |
Since isp output is YUV420, it will crash when calling .getCvFrame(). You could either resize the frame to 600x450 (so height is divisible by 3) on line 9,
or uncomment the line 8, so frame gets converted to BGR on the device itself.