DepthAI Hardware Documentation¶
Each device’s documentation includes an overview, getting started guide, images and project files (such as datasheets), Altium design files, 3D models, and mechanical models.
USB Designs¶
These are our most popular devices. Brought to market by a successful KickStarter campaign, OAK-D and OAK-1 products have been solving real-world problems since 2019. USB connection is great for development - it’s easy to use and allows up to 10Gbps throughput.
OAK-D Lite |
OAK-D S2 |
OAK-D Pro |
---|---|---|
![]() |
![]() |
![]() |
OAK-D Short Range |
OAK-D |
OAK-D Long Range |
---|---|---|
![]() |
![]() |
![]() |
OAK-1 Lite W |
OAK-1 W |
OAK-D W |
OAK-D Pro W |
---|---|---|---|
![]() |
![]() |
![]() |
![]() |
OAK-1 Lite |
OAK-1 |
OAK-1 Max |
---|---|---|
![]() |
![]() |
![]() |
PoE Designs¶
PoE devices are similar to USB devices, but instead of USB they have PoE connectivity and also feature on-board flash, so you can run pipelines in standalone mode.
OAK-D PoE |
OAK-D Pro PoE |
OAK-D Pro W PoE |
OAK-D Short Range PoE |
---|---|---|---|
![]() |
![]() |
![]() |
![]() |
OAK-1 PoE |
OAK-1 W PoE |
OAK-D S2 PoE |
OAK-D W PoE |
---|---|---|---|
![]() |
![]() |
![]() |
![]() |
Modular Camera Designs¶
The OAK FFC line is great for prototyping flexibility. Since cameras are modular, you can place them at various stereo baselines. This flexibility comes with a trade: you have to figure out how/where you will mount them, and then once mounted, perform a stereo calibration. This is not a TON of work, so keep in mind that these aren’t “plug and play” like other options. Instead, they are more for applications that require custom mounting, custom baseline, or custom orientation of the cameras.
OAK-FFC 3P |
OAK-FFC 4P |
OAK-FFC 4P PoE |
FFC Camera modules |
---|---|---|---|
![]() |
![]() |
![]() |
![]() |
OAK-FFC IMX378 |
OAK-FFC OV9282 |
OAK-FFC IMX582 |
OAK-FFC ToF 33D |
---|---|---|---|
![]() |
![]() |
![]() |
![]() |
System on Module (SoM) Designs¶
A SoM is perfect for integrating the power of DepthAI into your own products, or to customize one of our open-source hardware designs as you see fit.
OAK-SoM |
OAK-SoM Pro |
OAK-SoM MAX |
---|---|---|
![]() |
![]() |
![]() |
Other Designs¶
OAK Thermal (OAK-T) |
OAK-D CM4 |
OAK-D CM4 PoE |
rae Robot |
---|---|---|---|
![]() |
![]() |
![]() |
![]() |
Accessories¶
FSYNC Y-Adapter |
OAK Y-Adapter |
---|---|
![]() |
![]() |
Some older models can be found here.