FFC Camera Visualization ======================== This example shows how to use the `Camera` component to display the camera feed from the FFC camera. For FFC, the camera board socket must be specified. In our case the cameras are connected to socket A, B and C. After setting the resolution to 1200p and downscaling using ISP to 800p, the camera feed is displayed in a window. .. include:: /includes/blocking_behavior.rst Setup ##### .. include:: /includes/install_from_pypi.rst Pipeline ######## .. image:: /_static/images/pipelines/cam_ffc.png :alt: Pipeline graph Source Code ########### .. tabs:: .. tab:: Python Also `available on GitHub `__ .. literalinclude:: ../../../../examples/CameraComponent/cam_ffc.py :language: python :linenos: .. include:: /includes/footer-short.rst