Camera Control ============== This example shows how to use DepthAI SDK to control the color camera parameters. .. code-block:: Control: key[dec/inc] min..max exposure time: I O 1..33000 [us] sensitivity iso: K L 100..1600 To go back to auto controls: 'E' - autoexposure Demo #### .. image:: /_static/images/demos/sdk_camera_control.gif :alt: Camera Control Demo Setup ##### .. include:: /includes/install_from_pypi.rst Pipeline ######## .. image:: /_static/images/pipelines/camera_control.png :alt: Pipeline graph Source Code ########### .. tabs:: .. tab:: Python Also `available on GitHub `__ .. literalinclude:: ../../../../examples/CameraComponent/camera_control.py :language: python :linenos: .. include:: /includes/footer-short.rst