Preview All Cameras =================== This example shows how to set up a pipeline that outputs a a preview for each camera currently connected (and available) to the device. The preview is displayed in a window on the host machine. If run on OAK-D devices, this example does the same thing as the ``sdk_camera_preview`` example. .. include:: /includes/blocking_behavior.rst Demo #### .. image:: /_static/images/demos/sdk_preview_all_cameras.png :alt: Camera Preview Demo Setup ##### .. include:: /includes/install_from_pypi.rst Pipeline ######## .. image:: /_static/images/pipelines/preview_all_cameras.png :alt: Pipeline graph Source Code ########### .. tabs:: .. tab:: Python Also `available on GitHub `__ .. literalinclude:: ../../../../examples/CameraComponent/preview_all_cameras.py :language: python :linenos: .. include:: /includes/footer-short.rst