Stereo Control ============== This example shows how to change stereo parameter such as confidence threshold, median filter and decimating factor on the fly. .. code-block:: Control: key[dec/inc] min..max Confidence threshold: I O 1....255 Switches: 'K' - Switch median filter '1' - Switch to decimation factor 1 '2' - Switch to decimation factor 2 '3' - Switch to decimation factor 3 .. include:: /includes/blocking_behavior.rst Demo #### .. image:: /_static/images/demos/sdk_camera_control.gif :alt: Camera Preview Demo Setup ##### .. include:: /includes/install_from_pypi.rst Pipeline ######## .. image:: /_static/images/pipelines/stereo_control.png :alt: Pipeline graph Source Code ########### .. tabs:: .. tab:: Python Also `available on GitHub `_. .. literalinclude:: ../../../../examples/StereoComponent/stereo_control.py :language: python :linenos: .. include:: /includes/footer-short.rst