Collision Avoidance =================== This example shows how to set up a depth based collision avoidance system for proximity. This can be used with supervised robotic operation where the goal is to limit the robot's speed when a person is detected in front of it. .. include:: /includes/blocking_behavior.rst Demo #### .. image:: /_static/images/demos/sdk_collision_avoidance.gif :alt: Collision Avoidance Demo Setup ##### .. include:: /includes/install_from_pypi.rst Pipeline ######## .. image:: /_static/images/pipelines/collision_avoidance.png :alt: Pipeline graph Source Code ########### .. tabs:: .. tab:: Python Also `available on GitHub `_. .. literalinclude:: ../../../../examples/mixed/collision_avoidance.py :language: python :linenos: .. include:: /includes/footer-short.rst