Switch Between Models ===================== This example shows how to switch between models on the fly. It uses script node to alter pipeline flow (either to use the yolo model or the mobilenet model). Setup ##### .. include:: /includes/install_from_pypi.rst Pipeline ######## .. image:: /_static/images/pipelines/switch_between_models.png :alt: Pipeline graph Source Code ########### .. tabs:: .. tab:: Python Also `available on GitHub `_. .. literalinclude:: ../../../../examples/mixed/switch_between_models.py :language: python :linenos: .. include:: /includes/footer-short.rst