NNComponent¶
NNComponent abstracts sourcing & decoding AI models, creating a DepthAI API node for neural inferencing, object tracking, and MultiStage pipelines setup. It also supports Roboflow integration.
DepthAI API nodes¶
For neural inference, NNComponent will use DepthAI API node:
If we are using MobileNet-SSD based AI model, this component will create MobileNetDetectionNetwork (or MobileNetSpatialDetectionNetwork if
spatialargument is set).If we are using YOLO based AI model, this component will create YoloDetectionNetwork (or YoloSpatialDetectionNetwork if
spatialargument is set).If it’s none of the above, component will create NeuralNetwork node.
If tracker argument is set and we have YOLO/MobileNet-SSD based model, this component will also create ObjectTracker node,
and connect the two nodes togeter.
Usage¶
from depthai_sdk import OakCamera, ResizeMode
with OakCamera(recording='cars-tracking-above-01') as oak:
color = oak.create_camera('color')
nn = oak.create_nn('vehicle-detection-0202', color, tracker=True)
nn.config_nn(resize_mode='stretch')
oak.visualize([nn.out.tracker, nn.out.passthrough], fps=True)
oak.start(blocking=True)
Component outputs¶
main- Default output. Streams NN results and high-res frames that were downscaled and used for inferencing. Produces DetectionPacket or TwoStagePacket (if it’s 2. stage NNComponent).passthrough- Default output. Streams NN results and passthrough frames (frames used for inferencing). Produces DetectionPacket or TwoStagePacket (if it’s 2. stage NNComponent).spatials- Streams depth and bounding box mappings (SpatialDetectionNework.boundingBoxMapping). Produces SpatialBbMappingPacket.twostage_crops- Streams 2. stage cropped frames to the host. Produces FramePacket.tracker- Streams ObjectTracker’s tracklets and high-res frames that were downscaled and used for inferencing. Produces TrackerPacket.nn_data- Streams NN raw output. Produces NNDataPacket.
Decoding outputs¶
NNComponent allows user to define their own decoding functions. There is a set of standardized outputs:
Note
This feature is still in development and is not guaranteed to work correctly in all cases.
Example usage:
import numpy as np
from depthai import NNData
from depthai_sdk import OakCamera
from depthai_sdk.classes import Detections
def decode(nn_data: NNData):
layer = nn_data.getFirstLayerFp16()
results = np.array(layer).reshape((1, 1, -1, 7))
dets = Detections(nn_data)
for result in results[0][0]:
if result[2] > 0.5:
dets.add(result[1], result[2], result[3:])
return dets
def callback(packet: DetectionPacket, visualizer: Visualizer):
detections: Detections = packet.img_detections
...
with OakCamera() as oak:
color = oak.create_camera('color')
nn = oak.create_nn(..., color, decode_fn=decode)
oak.visualize(nn, callback=callback)
oak.start(blocking=True)
Reference¶
General (standarized) NN outputs, to be used for higher-level abstractions (eg. automatic visualization of results). “SDK supported NN models” will have to have standard NN output, so either dai.ImgDetections, or one of the outputs below. If the latter, model json config will incldue handler.py logic for decoding to the standard NN output. These will be integrated into depthai-core, bonus points for on-device decoding of some popular models.
-
class
depthai_sdk.classes.nn_results.Detection(img_detection: Union[NoneType, depthai.ImgDetection, depthai.SpatialImgDetection], label_str: str, confidence: float, color: Tuple[int, int, int], bbox: depthai_sdk.visualize.bbox.BoundingBox, angle: Union[int, NoneType], ts: Union[datetime.timedelta, NoneType])¶ -
-
bbox: depthai_sdk.visualize.bbox.BoundingBox¶
-
ts: Optional[datetime.timedelta]¶
-
property
top_left¶
-
property
bottom_right¶
-
-
class
depthai_sdk.classes.nn_results.TrackingDetection(img_detection: Union[NoneType, depthai.ImgDetection, depthai.SpatialImgDetection], label_str: str, confidence: float, color: Tuple[int, int, int], bbox: depthai_sdk.visualize.bbox.BoundingBox, angle: Union[int, NoneType], ts: Union[datetime.timedelta, NoneType], tracklet: depthai.Tracklet, filtered_2d: depthai_sdk.visualize.bbox.BoundingBox, filtered_3d: depthai.Point3f, speed: Union[float, NoneType])¶ -
tracklet: depthai.Tracklet¶
-
filtered_2d: depthai_sdk.visualize.bbox.BoundingBox¶
-
filtered_3d: depthai.Point3f¶
-
property
speed_kmph¶
-
property
speed_mph¶
-
-
class
depthai_sdk.classes.nn_results.TwoStageDetection(img_detection: Union[NoneType, depthai.ImgDetection, depthai.SpatialImgDetection], label_str: str, confidence: float, color: Tuple[int, int, int], bbox: depthai_sdk.visualize.bbox.BoundingBox, angle: Union[int, NoneType], ts: Union[datetime.timedelta, NoneType], nn_data: depthai.NNData)¶ -
nn_data: depthai.NNData¶
-
-
class
depthai_sdk.classes.nn_results.GenericNNOutput(nn_data)¶ Generic NN output, to be used for higher-level abstractions (eg. automatic visualization of results).
-
getTimestamp()¶ - Return type
-
-
class
depthai_sdk.classes.nn_results.Detections(nn_data, is_rotated=False)¶ Detection results containing bounding boxes, labels and confidences. Optionally can contain rotation angles.
-
class
depthai_sdk.classes.nn_results.SemanticSegmentation(nn_data, mask)¶ Semantic segmentation results, with a mask for each class.
Examples: DeeplabV3, Lanenet, road-segmentation-adas-0001.
-
mask: List[numpy.ndarray]¶
-
-
class
depthai_sdk.classes.nn_results.ImgLandmarks(nn_data, landmarks=None, landmarks_indices=None, pairs=None, colors=None)¶ Landmarks results, with a list of landmarks and pairs of landmarks to draw lines between.
Examples: human-pose-estimation-0001, openpose2, facial-landmarks-68, landmarks-regression-retail-0009.
-
class
depthai_sdk.classes.nn_results.InstanceSegmentation(nn_data, masks, labels)¶ Instance segmentation results, with a mask for each instance.
-
masks: List[numpy.ndarray]¶
-