Recording¶
OakCamera allows users to easily record video streams so the scene can later be fully replayed (see Replaying documentation), including reconstructing the stereo depth perception.
The script below will save color, left, and right H265 encoded streams into video files. Frames are synchronized (via timestamps) before being saved.
from depthai_sdk import OakCamera, RecordType
with OakCamera() as oak:
color = oak.create_camera('color', resolution='1080P', fps=20, encode='H265')
left = oak.create_camera('left', resolution='800p', fps=20, encode='H265')
right = oak.create_camera('right', resolution='800p', fps=20, encode='H265')
# Synchronize & save all (encoded) streams
oak.record([color.out.encoded, left.out.encoded, right.out.encoded], './', RecordType.VIDEO)
# Show color stream
oak.visualize([color.out.camera], scale=2/3, fps=True)
oak.start(blocking=True)
Recording pipeline of the script above¶
After 20 seconds we stopped the recording and SDK printed the location of saved files (./1-18443010D116631200 in our case):
Mode LastWriteTime Length Name
---- ------------- ------ ----
-a---- 10/3/2022 12:50 PM 9281 calib.json
-a---- 10/3/2022 12:51 PM 19172908 color.mp4
-a---- 10/3/2022 12:51 PM 15137490 left.mp4
-a---- 10/3/2022 12:51 PM 15030761 right.mp4
This depthai-recording can then be used next time to reconstruct the whole scene using the Replaying feature.
Supported recording types¶
1. Video¶
This option will write each stream separately to a video file. There are three options for saving these files:
If we are saving unencoded frames SDK will use
cv2.VideoWriterclass to save these streams into.avifile.If we are saving encoded streams and we have
avinstalled (PyAv library) SDK will save encoded streams directly to.mp4container. This will allow you to watch videos with a standard video player. There’s no decoding/encoding (or converting) happening on the host computer and host CPU/GPU/RAM usage is minimal. More information here.Otherwise SDK will save encoded streams to files (eg.
color.mjpeg) and you can use ffmpeg or mkvmerge to containerize the stream so it’s viewable by most video players. More information here.
200 frames from 4K color camera using different encoding options (MJPEG, H.264, H.265) using av:
2. Rosbag¶
Currently, we only support recording depth to the rosbag (recording.bag). In the future we will also support color (which is depth aligned)
stream and mono streams. You can open the rosbag with the RealSense Viewer to view the depth:
3. MCAP recording¶
An alternative to Rosbags are mcap files which can be viewed with Foxglove studio. You can find MCAP recording example here. Currently supported streams:
MJPEG encoded color/left/right/disparity. Lossless MJPEG/H264/H265 aren’t supported by Foxglove Studio.
Non-encoded color/left/right/disparity/depth frames.
Pointcloud, enable with
recorder.config_mcap(pointcloud=True). It converts depth frame to pointcloud on the host.
Standalone Foxglove studio streaming demo can be found here.
Available topics in Foxglove Studio from MCAP recorded by mcap-recording.py example¶