Packets¶
Packets are synchronized collections of one or more DepthAI messages. They are used internally for visualization and also forwarded to the callback function if the user:
Specified a callback for visualizing of an output via
OakCamera.visualize(..., callback=fn).Used callback output via
OakCamera.callback(..., callback=fn, enable_visualizer=True).
API Usage¶
OakCamera.visualize(): In the example below SDK won’t show the frame to the user, but instead it will send the packet to the callback function. SDK will draw detections (bounding boxes, labels) on thepacket.frame.OakCamera.callback(): This will also sendDetectionPacketto the callback function, the only difference is that the SDK won’t draw on the frame, so you can draw detections on the frame yourself.
Note
If you specify callback function in OakCamera.visualize(), you need to trigger drawing of detections yourself via Visualizer.draw() method.
import cv2
from depthai_sdk import OakCamera
from depthai_sdk.classes import DetectionPacket
with OakCamera() as oak:
color = oak.create_camera('color')
nn = oak.create_nn('mobilenet-ssd', color)
# Callback
def cb(packet: DetectionPacket):
print(packet.img_detections)
cv2.imshow(packet.name, packet.frame)
# 1. Callback after visualization:
oak.visualize(nn.out.main, fps=True, callback=cb)
# 2. Callback:
oak.callback(nn.out.main, callback=cb, enable_visualizer=True)
oak.start(blocking=True)
Reference¶
FramePacket¶
SpatialBbMappingPacket¶
-
class
depthai_sdk.classes.packets.SpatialBbMappingPacket(name, msg, spatials, disp_scale_factor)¶ Output from Spatial Detection nodes - depth frame + bounding box mappings. Inherits FramePacket.
-
prepare_visualizer_objects(vis)¶ Prepare visualizer objects (boxes, lines, text, etc.), so visualizer can draw them on the frame.
- Parameters
visualizer – Visualizer object.
- Return type
-
DetectionPacket¶
-
class
depthai_sdk.classes.packets.DetectionPacket(name, msg, dai_msg, bbox)¶ Output from Detection Network nodes - image frame + image detections. Inherits FramePacket.
-
prepare_visualizer_objects(vis)¶ Prepare visualizer objects (boxes, lines, text, etc.), so visualizer can draw them on the frame.
- Parameters
visualizer – Visualizer object.
- Return type
-
NNDataPacket¶
TrackerPacket¶
-
class
depthai_sdk.classes.packets.TrackerPacket(name, msg, tracklets, bbox)¶ Output of Object Tracker node. Tracklets + Image frame. Inherits FramePacket.
-
prepare_visualizer_objects(visualizer)¶ Prepare visualizer objects (boxes, lines, text, etc.), so visualizer can draw them on the frame.
- Parameters
visualizer (depthai_sdk.visualize.visualizer.Visualizer) – Visualizer object.
- Return type
-
TwoStagePacket¶
-
class
depthai_sdk.classes.packets.TwoStagePacket(name, msg, img_detections, nn_data, labels, bbox)¶ Output of 2-stage NN pipeline; Image frame, Image detections and multiple NNData results. Inherits DetectionPacket.
IMUPacket¶
-
class
depthai_sdk.classes.packets.IMUPacket(name, packet, rotation=None)¶ -
get_imu_vals()¶ Returns imu values in a tuple. Returns in format (accelerometer_values, gyroscope_values, quaternion, magnetometer_values)
- Return type
Tuple[Sequence, Sequence, Sequence, Sequence]
-
get_timestamp()¶ - Return type
-