Visualizer¶
DepthAI SDK visualizer serves as a tool to visualize the output of the DepthAI pipeline.
It can be used to visualize the output of the camera, neural network, depth and disparity map, the rectified streams, the spatial location of the detected objects, and more.
Getting Started¶
Visualizer is created upon calling
OakCamera.visualize(), which returns Visualizer instance.
Once it is created, the visualizer configs can be modified using output(),
stereo(),
text(),
detections(),
tracking() methods.
Example how Visualizer can be created:
from depthai_sdk import OakCamera
with OakCamera() as oak:
cam = oak.create_camera('color')
visualizer = oak.visualize(cam.out.main)
oak.start(blocking=True)
Visualizer is primarily used alongside with Packets
in depthai_sdk.oak_outputs module.
Configs¶
Visualizer is configurable via
VisConfig that consists of five auxiliary configs:
OutputConfig,
StereoConfig,
TextConfig,
DetectionConfig,
and TrackingConfig.
Each config’s type has its own set of parameters, which effects how the corresponding object will be visualized.
There are the following methods for modifying the default configuration:
output(),
stereo(),
text(),
detections(),
tracking().
The arguments should be passed as key-value arguments with the same signature as the corresponding config,
e.g., Visualizer.text(font_size=2, font_color=(255,123,200)).
The modified configuration will be applied to every created objects. The methods support
fluent interface and can be chained, e.g., Visualizer.text(font_size=2).detections(color=(255, 0, 0)).
Example how to configure the visualizer:
visualizer = oak.visualize(camera.out.main)
visualizer.detections(
bbox_style=BboxStyle.RECTANGLE,
label_position=TextPosition.MID,
).text(
auto_scale=True
)
Objects¶
Visualizer operates with objects. Objects can be seen as a hierarchical structure.
The root object is self, and the children are the list of the created objects.
add_child should be used to add the object to the children list.
The parent object shares the config and frame shape with all children.
All objects must be derived from GenericObject.
Implemented objects:
VisCircle,
Objects can be added to the visualizer using the following methods:
Create your own object¶
If the provided functionality is not enough, you can create your own object. To do so, you need to create a class
derived from GenericObject and implement the
prepare,
serialize,
and draw methods.
The draw method should draw the object on the passed frame argument.
class YourOwnObject:
def __init__(self, ...):
...
def prepare(self) -> None:
...
def serialize(self) -> str:
...
def draw(self, frame) -> None:
...
with OakCamera() as oak:
cam = oak.create_camera(...)
visualizer = cam.visualize(cam.out.main)
visualizer.add_object(YourOwnObject(...))
Example usage¶
The following script will visualize the output of face detection model:
from depthai_sdk import OakCamera
from depthai_sdk.visualize.configs import BboxStyle, TextPosition
with OakCamera() as oak:
camera = oak.create_camera('color')
det = oak.create_nn('face-detection-retail-0004', camera)
visualizer = oak.visualize(det.out.main, fps=True)
visualizer.detections(
color=(0, 255, 0),
thickness=2,
bbox_style=BboxStyle.RECTANGLE,
label_position=TextPosition.MID,
).text(
font_color=(255, 255, 0),
auto_scale=True
).tracking(
line_thickness=5
)
oak.start(blocking=True)
Serialization¶
The visualizer provides a way to serialize the output objects to JSON, which can be used for further processing.
JSON schemas¶
General config¶
{
"frame_shape": {
"type": "array",
"items": {
"type": "integer"
},
"description": "Frame shape in (height, width) format."
},
"config": {
"type": "object",
"output": {
"img_scale": {
"type": "number",
"minimum": 0.0,
"maximum": 1.0,
"default": 1.0,
"description": "Scale of output image."
},
"show_fps": {
"type": "boolean",
"default": false,
"description": "Show FPS on output image."
},
"clickable": {
"type": "boolean",
"default": false,
"description": "Show disparity or depth value on mouse hover."
}
},
"stereo": {
"type": "object",
"colorize": {
"type": "integer",
"default": 2,
"description": "cv2 colormap."
},
"colormap": {
"type": "integer",
"default": 2,
"description": "0 - gray, 1 - color, 2 - blended color and depth."
},
"wls_filter": {
"type": "boolean",
"default": false
},
"wls_lambda": {
"type": "number",
"default": 8000.0
},
"wls_sigma": {
"type": "number",
"default": 1.5
}
},
"detection": {
"type": "object",
"thickness": {
"type": "integer",
"default": 1
},
"fill_transparency": {
"type": "number",
"default": 0.15,
"minimum": 0.0,
"maximum": 1.0,
"description": "Transparency of bbox fill."
},
"box_roundness": {
"type": "integer",
"default": 0,
"description": "Roundness of bbox corners, used only when bbox_style is set to BboxStyle.ROUNDED_*."
},
"color": {
"type": "array",
"items": {
"type": "integer"
},
"default": [0, 255, 0],
"description": "Default bbox color in RGB format."
},
"bbox_style": {
"type": "integer",
"default": 0,
"description": "``depthai_sdk.visualize.configs.BBoxStyle`` enum value."
},
"line_width": {
"type": "number",
"default": 0.5,
"minimum": 0.0,
"maximum": 1.0,
"description": "Horizontal line width of bbox."
},
"line_height": {
"type": "number",
"default": 0.5,
"minimum": 0.0,
"maximum": 1.0,
"description": "Vertical line height of bbox."
},
"hide_label": {
"type": "boolean",
"default": false,
"description": "Hide class label on output image."
},
"label_position": {
"type": "integer",
"default": 0,
"description": "``depthai_sdk.visualize.configs.TextPosition`` enum value."
},
"label_padding": {
"type": "integer",
"default": 10,
"description": "Padding between label and bbox."
}
},
"text": {
"font_face": {
"type": "integer",
"default": 0,
"description": "cv2 font face."
},
"font_color": {
"type": "array",
"items": {
"type": "integer"
},
"default": [255, 255, 255],
"description": "Font color in RGB format."
},
"font_transparency": {
"type": "number",
"default": 0.5,
"minimum": 0.0,
"maximum": 1.0
},
"font_scale": {
"type": "number",
"default": 1.0
},
"font_thickness": {
"type": "integer",
"default": 2
},
"font_position": {
"type": "integer",
"default": 0,
"description": "``depthai_sdk.visualize.configs.TextPosition`` enum value."
},
"bg_transparency": {
"type": "number",
"default": 0.5,
"minimum": 0.0,
"maximum": 1.0,
"description": "Text outline transparency."
},
"bg_color": {
"type": "array",
"items": {
"type": "integer"
},
"default": [0, 0, 0],
"description": "Text outline color in RGB format."
},
"line_type": {
"type": "integer",
"default": 16,
"description": "cv2 line type."
},
"auto_scale": {
"type": "boolean",
"default": true,
"description": "Automatically scale font size based on bbox size."
}
},
"tracking": {
"max_length": {
"type": "integer",
"default": -1,
"description": "Maximum length of tracking line, -1 for infinite."
},
"deletion_lost_threshold": {
"type": "integer",
"default": 5,
"description": "Number of frames after which lost track is deleted."
},
"line_thickness": {
"type": "integer",
"default": 1
},
"fading_tails": {
"type": "boolean",
"default": false,
"description": "Enable fading tails - reduces line thickness over time."
},
"line_color": {
"type": "array",
"items": {
"type": "integer"
},
"default": [255, 255, 255],
"description": "Tracking line color in RGB format."
},
"line_type": {
"type": "integer",
"default": 16,
"description": "cv2 line type."
}
},
"circle": {
"thickness": {
"type": "integer",
"default": 1
},
"color": {
"type": "array",
"items": {
"type": "integer"
},
"default": [0, 255, 0],
"description": "Circle color in RGB format."
},
"line_type": {
"type": "integer",
"default": 16,
"description": "cv2 line type."
}
}
},
"objects": {
"type": "array",
"items": {
"type": "object"
},
"description": "Array of objects (e.g. detection, text, line).",
"default": []
}
}
Objects¶
Detection:
{
"type": "detections",
"detections": {
"type": "array",
"items": {
"type": "object",
"bbox": {
"type": "array",
"items": {
"type": "number"
},
"description": "bbox absolute coordinates in format [x1, y1, x2, y2]"
},
"label": {
"type": "string",
"description": "class label"
},
"color": {
"type": "array",
"items": {
"type": "integer"
},
"description": "bbox color in RGB format"
}
}
},
"children": {
"type": "array",
"items": {
"type": "object"
},
"description": "array of child objects (e.g. detection, text, line)",
"default": []
}
}
Text:
{
"type": "text",
"text": {
"type": "plain_text"
},
"coords": {
"type": "array",
"items": {
"type": "number"
},
"description": "The absolute coordinates of the text in the format (x1, y1)."
}
}
Line:
{
"type": "line",
"pt1": {
"type": "array",
"items": {
"type": "number"
},
"description": "Absolute (x, y) coordinates of the first point."
},
"pt2": {
"type": "array",
"items": {
"type": "number"
},
"description": "Absolute (x, y) coordinates of the second point."
},
"children": {
"type": "array",
"items": {
"type": "object"
},
"description": "array of child objects (e.g. detection, text, line).",
"default": []
}
}
Example JSON output¶
{
"frame_shape": [720, 1280],
"config": {
"output": {
"img_scale": 1.0,
"show_fps": false,
"clickable": true
},
"stereo": {
"colorize": 2,
"colormap": 2,
"wls_filter": false,
"wls_lambda": 8000,
"wls_sigma": 1.5
},
"detection": {
"thickness": 1,
"fill_transparency": 0.15,
"box_roundness": 0,
"color": [0, 255, 0],
"bbox_style": 0,
"line_width": 0.5,
"line_height": 0.5,
"hide_label": false,
"label_position": 0,
"label_padding": 10
},
"text": {
"font_face": 0,
"font_color": [255, 255, 255],
"font_transparency": 0.5,
"font_scale": 1.0,
"font_thickness": 2,
"font_position": 0,
"bg_transparency": 0.5,
"bg_color": [0, 0, 0],
"line_type": 16,
"auto_scale": true
},
"tracking": {
"max_length": -1,
"deletion_lost_threshold": 5,
"line_thickness": 1,
"fading_tails": false,
"line_color": [255, 255, 255],
"line_type": 16
},
"circle": {
"thickness": 1,
"color": [255, 255, 255],
"line_type": 16
}
},
"objects": [
{
"type": "detections",
"detections": [
{
"bbox": [101, 437, 661, 712],
"label": "laptop",
"color": [210, 167, 218]
}
],
"children": [
{
"type": "text",
"text": "Laptop",
"coords": [111, 469]
}
]
}
]
}
References¶
-
class
depthai_sdk.visualize.visualizer.Visualizer(scale=None, fps=False)¶ -
add_object(obj)¶ Call set_config, set_frame_shape and prepare for the object and add it to the list of objects. :param obj: The object to add.
- Returns
self
- Parameters
- Return type
-
add_bbox(bbox, color=None, thickness=None, bbox_style=None, label=None)¶ Add a bounding box to the visualizer.
- Parameters
bbox (depthai_sdk.visualize.bbox.BoundingBox) – Bounding box.
label (Optional[str]) – Label for the detection.
thickness (Optional[int]) – Bounding box thickness.
color (Optional[Tuple[int, int, int]]) – Bounding box color (RGB).
bbox_style (Optional[depthai_sdk.visualize.configs.BboxStyle]) – Bounding box style (one of depthai_sdk.visualize.configs.BboxStyle).
- Returns
self
- Return type
-
add_detections(detections, normalizer=None, label_map=None, spatial_points=None, label_color=None, label_background_color=None, label_background_transparency=None, is_spatial=False, bbox=None)¶ Add detections to the visualizer.
- Parameters
detections (List[Union[depthai.ImgDetection, depthai.Tracklet]]) – List of detections.
normalizer (Optional[depthai_sdk.visualize.bbox.BoundingBox]) – Normalizer object.
label_map (Optional[List[Tuple[str, Tuple]]]) – List of tuples (label, color).
spatial_points (Optional[List[depthai.Point3f]]) – List of spatial points. None if not spatial.
label_color (Optional[Tuple[int, int, int]]) – Color for the label.
label_background_color (Optional[Tuple[int, int, int]]) – Color for the label background.
label_background_transparency (Optional[float]) – Transparency for the label background.
is_spatial – Flag that indicates if the detections are spatial.
bbox (Optional[Union[numpy.ndarray, Tuple[int, int, int, int]]]) – Bounding box, if there’s a detection inside a bounding box.
- Returns
self
- Return type
-
add_text(text, coords=None, size=None, color=None, thickness=None, outline=True, background_color=None, background_transparency=0.5, bbox=None, position=<TextPosition.TOP_LEFT: 0>, padding=10)¶ Add text to the visualizer.
- Parameters
text (str) – Text.
size (Optional[int]) – Size of the text.
thickness (Optional[int]) – Thickness of the text.
outline (bool) – Flag that indicates if the text should be outlined.
background_color (Optional[Tuple[int, int, int]]) – Background color.
background_transparency (float) – Background transparency.
bbox (Optional[Union[numpy.ndarray, Tuple, depthai_sdk.visualize.bbox.BoundingBox]]) – Bounding box.
position (depthai_sdk.visualize.configs.TextPosition) – Position.
padding (int) – Padding.
- Returns
self
- Return type
-
add_trail(tracklets, label_map, bbox=None)¶ Add a trail to the visualizer.
- Parameters
tracklets (List[depthai.Tracklet]) – List of tracklets.
label_map (List[Tuple[str, Tuple]]) – List of tuples (label, color).
bbox (Optional[depthai_sdk.visualize.bbox.BoundingBox]) – Bounding box.
- Returns
self
- Return type
-
add_circle(coords, radius, color=None, thickness=None)¶ Add a circle to the visualizer.
-
add_line(pt1, pt2, color=None, thickness=None)¶ Add a line to the visualizer.
-
add_mask(mask, alpha)¶ Add a mask to the visualizer.
- Parameters
mask (numpy.ndarray) – Mask represented as uint8 numpy array.
alpha (float) – Transparency of the mask.
- Returns
self
-
drawn(frame)¶ Draw all objects on the frame if the platform is PC. Otherwise, serialize the objects and communicate with the RobotHub application.
- Parameters
frame (numpy.ndarray) – The frame to draw on.
- Returns
np.ndarray if the platform is PC, None otherwise.
- Return type
Optional[numpy.ndarray]
-
show(packet)¶ Show the packet on the screen.
-
serialize(force_reset=True)¶ Serialize all contained objects to JSON.
-
reset()¶ Clear all objects.
-
output(img_scale=None, show_fps=None)¶ Configure the output of the visualizer.
- Parameters
- Returns
self
- Return type
-
stereo(colorize=None, colormap=None, wls_filter=None, wls_lambda=None, wls_sigma=None, depth_score=None)¶
-
detections(thickness=None, fill_transparency=None, bbox_roundness=None, color=None, bbox_style=None, line_width=None, line_height=None, hide_label=None, label_position=None, label_padding=None)¶ Configure how bounding boxes will look like. :param thickness: Thickness of the bounding box. :param fill_transparency: Transparency of the bounding box. :param bbox_roundness: Roundness of the bounding box. :param color: Color of the bounding box. :param bbox_style: Style of the bounding box. :param line_width: Width of the bbox horizontal lines CORNERS or ROUNDED_CORNERS style is used. :param line_height: Height of the bbox vertical lines when CORNERS or ROUNDED_CORNERS style is used. :param hide_label: Flag that indicates if the label should be hidden. :param label_position: Position of the label. :param label_padding: Padding of the label.
- Returns
self
- Parameters
thickness (Optional[int]) –
fill_transparency (Optional[float]) –
bbox_roundness (Optional[float]) –
bbox_style (Optional[depthai_sdk.visualize.configs.BboxStyle]) –
line_width (Optional[float]) –
line_height (Optional[float]) –
hide_label (Optional[bool]) –
label_position (Optional[depthai_sdk.visualize.configs.TextPosition]) –
label_padding (Optional[int]) –
- Return type
-
text(font_face=None, font_color=None, font_transparency=None, font_scale=None, font_thickness=None, font_position=None, background_transparency=None, background_color=None, outline_color=None, line_type=None, auto_scale=None)¶ Configure how text will look like.
- Parameters
font_face (Optional[int]) – Font face (from cv2).
font_transparency (Optional[float]) – Font transparency.
font_scale (Optional[float]) – Font scale.
font_thickness (Optional[int]) – Font thickness.
font_position (Optional[depthai_sdk.visualize.configs.TextPosition]) – Font position.
background_transparency (Optional[float]) – Text background transparency.
background_color (Optional[Tuple[int, int, int]]) – Text background color.
outline_color (Optional[Tuple[int, int, int]]) – Outline color.
line_type (Optional[int]) – Line type (from cv2).
auto_scale (Optional[bool]) – Flag that indicates if the font scale should be automatically adjusted.
- Returns
self
- Return type
-
tracking(max_length=None, deletion_lost_threshold=None, line_thickness=None, fading_tails=None, show_speed=None, line_color=None, line_type=None, bg_color=None)¶ Configure how tracking trails will look like.
- Parameters
max_length (Optional[int]) – Maximum length of the trail (in pixels).
deletion_lost_threshold (Optional[int]) – Number of consequent LOST statuses after which the trail is deleted.
line_thickness (Optional[int]) – Thickness of the line.
fading_tails (Optional[bool]) – Flag that indicates if the tails should fade.
show_speed (Optional[bool]) – Flag that indicates if the speed should be shown.
line_color (Optional[Tuple[int, int, int]]) – Color of the line.
line_type (Optional[int]) – Type of the line (from cv2).
bg_color (Optional[Tuple[int, int, int]]) – Text background color.
- Returns
self
- Return type
-
property
frame_shape¶
-
close()¶
-
-
class
depthai_sdk.visualize.objects.GenericObject(config=VisConfig(output=OutputConfig(img_scale=1.0, show_fps=False, clickable=True), stereo=StereoConfig(colorize=<StereoColor.RGB: 2>, colormap=array([[[128, 0, 0]], [[132, 0, 0]], [[136, 0, 0]], [[140, 0, 0]], [[144, 0, 0]], [[148, 0, 0]], [[152, 0, 0]], [[156, 0, 0]], [[160, 0, 0]], [[164, 0, 0]], [[168, 0, 0]], [[172, 0, 0]], [[176, 0, 0]], [[180, 0, 0]], [[184, 0, 0]], [[188, 0, 0]], [[192, 0, 0]], [[196, 0, 0]], [[200, 0, 0]], [[204, 0, 0]], [[208, 0, 0]], [[212, 0, 0]], [[216, 0, 0]], [[220, 0, 0]], [[224, 0, 0]], [[228, 0, 0]], [[232, 0, 0]], [[236, 0, 0]], [[240, 0, 0]], [[244, 0, 0]], [[248, 0, 0]], [[252, 0, 0]], [[255, 0, 0]], [[255, 4, 0]], [[255, 8, 0]], [[255, 12, 0]], [[255, 16, 0]], [[255, 20, 0]], [[255, 24, 0]], [[255, 28, 0]], [[255, 32, 0]], [[255, 36, 0]], [[255, 40, 0]], [[255, 44, 0]], [[255, 48, 0]], [[255, 52, 0]], [[255, 56, 0]], [[255, 60, 0]], [[255, 64, 0]], [[255, 68, 0]], [[255, 72, 0]], [[255, 76, 0]], [[255, 80, 0]], [[255, 84, 0]], [[255, 88, 0]], [[255, 92, 0]], [[255, 96, 0]], [[255, 100, 0]], [[255, 104, 0]], [[255, 108, 0]], [[255, 112, 0]], [[255, 116, 0]], [[255, 120, 0]], [[255, 124, 0]], [[255, 128, 0]], [[255, 132, 0]], [[255, 136, 0]], [[255, 140, 0]], [[255, 144, 0]], [[255, 148, 0]], [[255, 152, 0]], [[255, 156, 0]], [[255, 160, 0]], [[255, 164, 0]], [[255, 168, 0]], [[255, 172, 0]], [[255, 176, 0]], [[255, 180, 0]], [[255, 184, 0]], [[255, 188, 0]], [[255, 192, 0]], [[255, 196, 0]], [[255, 200, 0]], [[255, 204, 0]], [[255, 208, 0]], [[255, 212, 0]], [[255, 216, 0]], [[255, 220, 0]], [[255, 224, 0]], [[255, 228, 0]], [[255, 232, 0]], [[255, 236, 0]], [[255, 240, 0]], [[255, 244, 0]], [[255, 248, 0]], [[255, 252, 0]], [[254, 255, 2]], [[250, 255, 6]], [[246, 255, 10]], [[242, 255, 14]], [[238, 255, 18]], [[234, 255, 22]], [[230, 255, 26]], [[226, 255, 30]], [[222, 255, 34]], [[218, 255, 38]], [[214, 255, 42]], [[210, 255, 46]], [[206, 255, 50]], [[202, 255, 54]], [[198, 255, 58]], [[194, 255, 62]], [[190, 255, 66]], [[186, 255, 70]], [[182, 255, 74]], [[178, 255, 78]], [[174, 255, 82]], [[170, 255, 86]], [[166, 255, 90]], [[162, 255, 94]], [[158, 255, 98]], [[154, 255, 102]], [[150, 255, 106]], [[146, 255, 110]], [[142, 255, 114]], [[138, 255, 118]], [[134, 255, 122]], [[130, 255, 126]], [[126, 255, 130]], [[122, 255, 134]], [[118, 255, 138]], [[114, 255, 142]], [[110, 255, 146]], [[106, 255, 150]], [[102, 255, 154]], [[ 98, 255, 158]], [[ 94, 255, 162]], [[ 90, 255, 166]], [[ 86, 255, 170]], [[ 82, 255, 174]], [[ 78, 255, 178]], [[ 74, 255, 182]], [[ 70, 255, 186]], [[ 66, 255, 190]], [[ 62, 255, 194]], [[ 58, 255, 198]], [[ 54, 255, 202]], [[ 50, 255, 206]], [[ 46, 255, 210]], [[ 42, 255, 214]], [[ 38, 255, 218]], [[ 34, 255, 222]], [[ 30, 255, 226]], [[ 26, 255, 230]], [[ 22, 255, 234]], [[ 18, 255, 238]], [[ 14, 255, 242]], [[ 10, 255, 246]], [[ 6, 255, 250]], [[ 1, 255, 254]], [[ 0, 252, 255]], [[ 0, 248, 255]], [[ 0, 244, 255]], [[ 0, 240, 255]], [[ 0, 236, 255]], [[ 0, 232, 255]], [[ 0, 228, 255]], [[ 0, 224, 255]], [[ 0, 220, 255]], [[ 0, 216, 255]], [[ 0, 212, 255]], [[ 0, 208, 255]], [[ 0, 204, 255]], [[ 0, 200, 255]], [[ 0, 196, 255]], [[ 0, 192, 255]], [[ 0, 188, 255]], [[ 0, 184, 255]], [[ 0, 180, 255]], [[ 0, 176, 255]], [[ 0, 172, 255]], [[ 0, 168, 255]], [[ 0, 164, 255]], [[ 0, 160, 255]], [[ 0, 156, 255]], [[ 0, 152, 255]], [[ 0, 148, 255]], [[ 0, 144, 255]], [[ 0, 140, 255]], [[ 0, 136, 255]], [[ 0, 132, 255]], [[ 0, 128, 255]], [[ 0, 124, 255]], [[ 0, 120, 255]], [[ 0, 116, 255]], [[ 0, 112, 255]], [[ 0, 108, 255]], [[ 0, 104, 255]], [[ 0, 100, 255]], [[ 0, 96, 255]], [[ 0, 92, 255]], [[ 0, 88, 255]], [[ 0, 84, 255]], [[ 0, 80, 255]], [[ 0, 76, 255]], [[ 0, 72, 255]], [[ 0, 68, 255]], [[ 0, 64, 255]], [[ 0, 60, 255]], [[ 0, 56, 255]], [[ 0, 52, 255]], [[ 0, 48, 255]], [[ 0, 44, 255]], [[ 0, 40, 255]], [[ 0, 36, 255]], [[ 0, 32, 255]], [[ 0, 28, 255]], [[ 0, 24, 255]], [[ 0, 20, 255]], [[ 0, 16, 255]], [[ 0, 12, 255]], [[ 0, 8, 255]], [[ 0, 4, 255]], [[ 0, 0, 255]], [[ 0, 0, 252]], [[ 0, 0, 248]], [[ 0, 0, 244]], [[ 0, 0, 240]], [[ 0, 0, 236]], [[ 0, 0, 232]], [[ 0, 0, 228]], [[ 0, 0, 224]], [[ 0, 0, 220]], [[ 0, 0, 216]], [[ 0, 0, 212]], [[ 0, 0, 208]], [[ 0, 0, 204]], [[ 0, 0, 200]], [[ 0, 0, 196]], [[ 0, 0, 192]], [[ 0, 0, 188]], [[ 0, 0, 184]], [[ 0, 0, 180]], [[ 0, 0, 176]], [[ 0, 0, 172]], [[ 0, 0, 168]], [[ 0, 0, 164]], [[ 0, 0, 160]], [[ 0, 0, 156]], [[ 0, 0, 152]], [[ 0, 0, 148]], [[ 0, 0, 144]], [[ 0, 0, 140]], [[ 0, 0, 136]], [[ 0, 0, 132]], [[ 0, 0, 128]]], dtype=uint8), wls_filter=False, wls_lambda=8000, wls_sigma=1.5, depth_score=False), detection=DetectionConfig(thickness=1, fill_transparency=0.15, box_roundness=0, color=(0, 255, 0), bbox_style=<BboxStyle.RECTANGLE: 0>, line_width=0.5, line_height=0.5, hide_label=False, label_position=<TextPosition.TOP_LEFT: 0>, label_padding=10), text=TextConfig(font_face=0, font_color=(255, 255, 255), font_transparency=0.5, font_scale=1.0, font_thickness=2, font_position=<TextPosition.TOP_LEFT: 0>, background_color=None, background_transparency=0.5, outline_color=(0, 0, 0), line_type=16, auto_scale=True), tracking=TrackingConfig(max_length=500, deletion_lost_threshold=5, line_thickness=1, fading_tails=False, line_color=(255, 255, 255), line_type=16, show_speed=False), circle=CircleConfig(thickness=1, color=(255, 255, 255), line_type=16)), frame_shape=None)¶ Generic object used by visualizer.
-
set_config(config)¶ Set the configuration for the current object.
- Parameters
config (depthai_sdk.visualize.configs.VisConfig) – instance of VisConfig.
- Returns
self
- Return type
-
set_frame_shape(frame_shape)¶ Set the incoming frame shape for the current object.
- Parameters
frame_shape (Tuple[int, ..]) – frame shape as a tuple of (height, width, channels).
- Returns
self
- Return type
-
prepare()¶ Prepare necessary data for drawing.
- Returns
self
- Return type
-
add_child(child)¶ Add a child object to the current object.
- Parameters
child (depthai_sdk.visualize.objects.GenericObject) – instance derived from GenericObject.
- Returns
self
- Return type
-
property
children¶ Get the children of the current object.
- Returns
List of children.
-
-
class
depthai_sdk.visualize.objects.VisDetections(detections, normalizer, label_map=None, label_color=None, label_background_color=None, label_background_transparency=None, spatial_points=None, is_spatial=False, parent_bbox=None)¶ Object that represents detections.
-
register_detection(bbox, label, color)¶ Register a detection.
-
prepare()¶ Prepare necessary data for drawing.
- Returns
self
- Return type
-
-
class
depthai_sdk.visualize.objects.VisText(text, coords=None, size=None, color=None, thickness=None, outline=True, background_color=None, background_transparency=0.5, bbox=None, position=<TextPosition.TOP_LEFT: 0>, padding=10)¶ Object that represents a text.
-
serialize()¶ Serialize the object to dict.
-
-
class
depthai_sdk.visualize.objects.VisLine(pt1, pt2, color=None, thickness=None)¶ Object that represents a line.
-
serialize()¶ Serialize the object to dict.
-
prepare()¶ Prepare necessary data for drawing.
- Returns
self
- Return type
-
-
class
depthai_sdk.visualize.objects.VisTrail(tracklets, label_map, bbox)¶ Object that represents a trail.
-
serialize()¶ Serialize the object to dict.
-
prepare()¶ Prepare necessary data for drawing.
- Returns
self
- Return type
-
groupby_tracklet()¶ Group tracklets by tracklet id.
- Returns
Dictionary of tracklets grouped by tracklet id.
-
-
class
depthai_sdk.visualize.configs.TextPosition(value)¶ Where on frame do we want to print text.
-
TOP_LEFT= 0¶
-
MID_LEFT= 1¶
-
BOTTOM_LEFT= 2¶
-
TOP_MID= 10¶
-
MID= 11¶
-
BOTTOM_MID= 12¶
-
TOP_RIGHT= 20¶
-
MID_RIGHT= 21¶
-
BOTTOM_RIGHT= 22¶
-
-
class
depthai_sdk.visualize.configs.BboxStyle(value)¶ How do we want to draw bounding box.
-
RECTANGLE= 0¶
-
CORNERS= 1¶
-
ROUNDED_RECTANGLE= 10¶
-
ROUNDED_CORNERS= 11¶
-
-
class
depthai_sdk.visualize.configs.StereoColor(value)¶ An enumeration.
-
GRAY= 1¶
-
RGB= 2¶
-
RGBD= 3¶
-
-
class
depthai_sdk.visualize.configs.OutputConfig(img_scale=1.0, show_fps=False, clickable=True)¶ Configuration for output of the visualizer.
-
class
depthai_sdk.visualize.configs.StereoConfig(colorize: depthai_sdk.visualize.configs.StereoColor = <StereoColor.RGB: 2>, colormap: numpy.ndarray = <factory>, wls_filter: bool = False, wls_lambda: float = 8000, wls_sigma: float = 1.5, depth_score: bool = False)¶ -
colorize: depthai_sdk.visualize.configs.StereoColor = 2¶
-
colormap: numpy.ndarray¶
-
-
class
depthai_sdk.visualize.configs.DetectionConfig(thickness=1, fill_transparency=0.15, box_roundness=0, color=(0, 255, 0), bbox_style=<BboxStyle.RECTANGLE: 0>, line_width=0.5, line_height=0.5, hide_label=False, label_position=<TextPosition.TOP_LEFT: 0>, label_padding=10)¶ Configuration for drawing bounding boxes.
-
bbox_style: depthai_sdk.visualize.configs.BboxStyle = 0¶
-
label_position: depthai_sdk.visualize.configs.TextPosition = 0¶
-
-
class
depthai_sdk.visualize.configs.TextConfig(font_face=0, font_color=(255, 255, 255), font_transparency=0.5, font_scale=1.0, font_thickness=2, font_position=<TextPosition.TOP_LEFT: 0>, background_color=None, background_transparency=0.5, outline_color=(0, 0, 0), line_type=16, auto_scale=True)¶ Configuration for drawing labels.
-
font_position: depthai_sdk.visualize.configs.TextPosition = 0¶
-
-
class
depthai_sdk.visualize.configs.TrackingConfig(max_length=500, deletion_lost_threshold=5, line_thickness=1, fading_tails=False, line_color=(255, 255, 255), line_type=16, show_speed=False)¶ Configuration for drawing tracking bounding boxes.
-
class
depthai_sdk.visualize.configs.SegmentationConfig(mask_alpha=0.5)¶ Configuration for drawing segmentation masks.
-
class
depthai_sdk.visualize.configs.CircleConfig(thickness=1, color=(255, 255, 255), line_type=16)¶ Configuration for drawing circles.
-
class
depthai_sdk.visualize.configs.VisConfig(output=<factory>, stereo=<factory>, detection=<factory>, text=<factory>, tracking=<factory>, circle=<factory>)¶ Configuration for visualizer.