Custom Decode Function¶
This example showcases the usage of custom decoding functions for the neural network component. More info is available inside the function itself.
Note
Visualization in current example is done with blocking behavor. This means that the program will halt at oak.start() until the window is closed.
This is done to keep the example simple. For more advanced usage, see Blocking behavior section.
Setup¶
Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai repository first and then run the script
git clone https://github.com/luxonis/depthai.git
cd depthai/
python3 install_requirements.py
For additional information, please follow our installation guide.
Pipeline¶
Source Code¶
Also available on GitHub.
1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31 32 33 34 35 36 37 38 39 40 41 42 | import blobconverter import numpy as np import depthai as dai from depthai_sdk import OakCamera from depthai_sdk.classes import Detections def decode(nn_data: dai.NNData) -> Detections: """ Custom decode function for the NN component. Decode function has to accept NNData argument. The return type should preferably be a class that inherits from depthai_sdk.classes.GenericNNOutput, which support visualization. But this is not required, i.e. the function can return arbitrary type. The decoded output can be accessed from the packet object in the callback function via packet.img_detections. """ layer = nn_data.getFirstLayerFp16() results = np.array(layer).reshape((1, 1, -1, 7)) dets = Detections(nn_data) for result in results[0][0]: if result[2] > 0.3: label = int(result[1]) conf = result[2] bbox = result[3:] det = dai.ImgDetection() det.confidence = conf det.label = label det.xmin = bbox[0] det.ymin = bbox[1] det.xmax = bbox[2] det.ymax = bbox[3] dets.detections.append(det) return dets with OakCamera() as oak: color = oak.create_camera('color') nn_path = blobconverter.from_zoo(name='person-detection-0200', version='2021.4', shaves=6) nn = oak.create_nn(nn_path, color, decode_fn=decode) oak.visualize(nn) oak.start(blocking=True) |