Switch Between Models¶
This example shows how to switch between models on the fly. It uses script node to alter pipeline flow (either to use the yolo model or the mobilenet model).
Setup¶
Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai repository first and then run the script
git clone https://github.com/luxonis/depthai.git
cd depthai/
python3 install_requirements.py
For additional information, please follow our installation guide.
Pipeline¶
![Pipeline graph](../../../_images/switch_between_models.png)
Source Code¶
Also available on GitHub.
1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31 32 33 34 35 36 37 38 39 40 41 42 43 44 45 46 47 48 49 50 51 52 53 54 55 56 57 58 59 60 | from depthai_sdk import OakCamera from depthai_sdk.classes.packets import DetectionPacket import depthai as dai import cv2 # We use callback, so we only have cv2 window for both models def cb(packet: DetectionPacket): frame = packet.visualizer.draw(packet.frame) cv2.imshow('Frame', frame) with OakCamera() as oak: color = oak.create_camera('color') script = oak.pipeline.create(dai.node.Script) # When Script node receives a message from the host it will switch streaming frames to another NN model script.setScript(""" i = 0 outputs = ['out1', 'out2'] while True: frame = node.io['frames'].get() switch = node.io['switch'].tryGet() if switch is not None: i += 1 if len(outputs) <= i: i = 0 node.io[outputs[i]].send(frame) """) color.stream.link(script.inputs['frames']) # We can have multiple models here, not just 2 object detection models nn1 = oak.create_nn('yolov6nr3_coco_640x352', input=script.outputs['out1']) nn1.config_nn(resize_mode='stretch') # otherwise, BB mappings will be incorrect nn2 = oak.create_nn('mobilenet-ssd', input=script.outputs['out2']) nn2.config_nn(resize_mode='stretch') # otherwise, BB mappings will be incorrect # We will send "switch" message via XLinkIn xin = oak.pipeline.create(dai.node.XLinkIn) xin.setStreamName('switch') xin.out.link(script.inputs['switch']) # We don't want syncing, we just want either of the model packets in the callback oak.visualize([nn1, nn2], fps=True, callback=cb) oak.visualize([nn1.out.passthrough, nn2.out.passthrough], fps=True) # oak.show_graph() oak.start() qin = oak.device.getInputQueue('switch') while True: key = oak.poll() if key == ord('s'): print('Switching NN model') qin.send(dai.Buffer()) elif key == ord('q'): break |