Custom Trigger Action¶
This example shows how to set custom action to be triggered when a certain event occurs. In this case, we will trigger an action when a person is detected in the frame. The action will save the exact frame to a file.
Note
Visualization in current example is done with blocking behavor. This means that the program will halt at oak.start() until the window is closed.
This is done to keep the example simple. For more advanced usage, see Blocking behavior section.
Setup¶
Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai repository first and then run the script
git clone https://github.com/luxonis/depthai.git
cd depthai/
python3 install_requirements.py
For additional information, please follow our installation guide.
Pipeline¶
Source Code¶
Also available on GitHub.
1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31 32 33 34 35 36 37 38 39 40 41 42 43 | from pathlib import Path from typing import Dict import cv2 from depthai_sdk import OakCamera, FramePacket from depthai_sdk.trigger_action import Action, DetectionTrigger class MyAction(Action): """ Saves the latest frame from the input stream to a file. """ def __init__(self, inputs, dir_path): super().__init__(inputs) self.dir_path = Path(dir_path) self.dir_path.mkdir(parents=True, exist_ok=True) self.latest_packets = None def activate(self): print('+', self.latest_packets) if self.latest_packets: for stream_name, packet in self.latest_packets.items(): print(f'Saving {stream_name} to {self.dir_path / f"{stream_name}.jpg"}') cv2.imwrite(str(self.dir_path / f'{stream_name}.jpg'), packet.frame) def on_new_packets(self, packets: Dict[str, FramePacket]) -> None: self.latest_packets = packets with OakCamera() as oak: color = oak.create_camera('color', '1080p') nn = oak.create_nn('mobilenet-ssd', color) oak.trigger_action( trigger=DetectionTrigger(input=nn, min_detections={'person': 1}, cooldown=30), action=MyAction(inputs=[nn], dir_path='./images/') # `action` can be Callable as well ) oak.start(blocking=True) |