Nnet manager
NNetManager is a class that is made to help you with setting up neural networks (NN). It is also responsible for all NN related functionalities.
It’s capable of creating appropriate nodes and connections, decoding neural network output automatically or by using external handler file.
Getting started
To get started we first have to know some things that the manager offers. Firstly the manager is responsible for running our NN, which means
that our manager will need a blob to work with. We can pass the blob to our NNetManager either with our BlobManager or we can pass the blob directly from the blobconverter module.
We now have our blob, now we need to declare our pipeline through which our NN will be receiving data. This step is best done with the help of
PipelineManager, as the manager already contains methods for NN nodes (addNN and setNnManager methods). After initializing all of that we are almost done.
For convenience we can use PreviewManager to parse our frames, but this step is not needed as te NNetManager is able to parse raw frames.
Bellow you can see 2 projects that use the NNetManager. Every major step is also commented for better understanding.
Face detection
1from depthai_sdk import Previews
2from depthai_sdk.managers import PipelineManager, PreviewManager, NNetManager, BlobManager
3import depthai as dai
4import cv2
5
6# create pipeline
7pm = PipelineManager()
8
9# define camera source (in this case color and change winow size to 600 x 500)
10pm.createColorCam(xout=True)
11
12# define project that you wish to run
13bm = BlobManager(zooName="face-detection-retail-0004")
14
15# define Neural network configs
16nm = NNetManager(inputSize=(300, 300), nnFamily="mobilenet")
17nn = nm.createNN(pipeline=pm.pipeline, nodes=pm.nodes, source=Previews.color.name,
18 blobPath=bm.getBlob(shaves=6, openvinoVersion=pm.pipeline.getOpenVINOVersion()))
19pm.addNn(nn)
20
21# connect to device
22with dai.Device(pm.pipeline) as device:
23 # define configs for above sources
24 pv = PreviewManager(display=[Previews.color.name])
25
26 # create stream and neural network queues
27 pv.createQueues(device)
28 nm.createQueues(device)
29 nnData = []
30
31 while True:
32 # read frames
33 pv.prepareFrames()
34 inNn = nm.outputQueue.tryGet()
35
36 if inNn is not None:
37 nnData = nm.decode(inNn)
38
39 # draw information on frame and show frame
40 nm.draw(pv, nnData)
41 pv.showFrames()
42
43 # end program with 'q'
44 if cv2.waitKey(1) == ord('q'):
45 break
In this above example we will use all classes that we learned before and run the face detection project.
First we define the pipeline and initialize the streams. After that we load in our blob (face-detection-retail-0004) and send it in to our NNetManager.
Every project has its own inputSize (desired NN input size, which should match input size defined in the network itself (width, height)) the and familyName (supported NN types / family names are YOLO and nobilenet).
After all that is initialized, we add our neural network to our pipeline and connect to our device. In our device we set our Previews, to see our stream and create our stream queues.
Like every other class that we covered, we need a loop, that will keep our project running, and in our loop, we get our frames, use our neural network to draw over our frames, and then we show them on the stream.
Outputs of our above program should look like this:
If our face is shown, our neural network detects it, but if we cover it, our neural network will not detect it.
Mobile net
1from depthai_sdk import Previews
2from depthai_sdk.managers import PipelineManager, PreviewManager, NNetManager, BlobManager
3import depthai as dai
4import cv2
5
6# create pipeline
7pm = PipelineManager()
8
9# define camera source (in this case color and change winow size to 600 x 500)
10pm.createColorCam(xout=True)
11
12# define project that you wish to run
13bm = BlobManager(zooName="mobilenet-ssd")
14
15# define Neural network configs
16nm = NNetManager(inputSize=(300, 300), nnFamily="mobilenet")
17nn = nm.createNN(pipeline=pm.pipeline, nodes=pm.nodes, source=Previews.color.name,
18 blobPath=bm.getBlob(shaves=6, openvinoVersion=pm.pipeline.getOpenVINOVersion()))
19pm.addNn(nn)
20
21# connect to device
22with dai.Device(pm.pipeline) as device:
23 # define configs for above sources
24 pv = PreviewManager(display=[Previews.color.name])
25
26 # create stream and neural network queues
27 pv.createQueues(device)
28 nm.createQueues(device)
29 nnData = []
30
31 while True:
32 # read frames
33 pv.prepareFrames()
34 inNn = nm.outputQueue.tryGet()
35
36 if inNn is not None:
37 nnData = nm.decode(inNn)
38
39 # draw information on frame and show frame
40 nm.draw(pv, nnData)
41 pv.showFrames()
42
43 # end program with 'q'
44 if cv2.waitKey(1) == ord('q'):
45 break
This example shows how to use the MobileNetSSD project. The code should be almost the same as the one that we used in the above example, with the only difference being
the blob. In this example we load the mobilenet-ssd blob and pass it to our neural network.
- class depthai_sdk.managers.NNetManager
Manager class handling all NN-related functionalities. It’s capable of creating appropriate nodes and connections, decoding neural network output automatically or by using external handler file.
- __init__(inputSize, nnFamily=None, labels=[], confidence=0.5, sync=False)
- Parameters
inputSize (tuple) – Desired NN input size, should match the input size defined in the network itself (width, height)
nnFamily (str, Optional) – type of NeuralNetwork to be processed. Supported:
"YOLO"andmobilenetlabels (list, Optional) – Allows to display class label instead of ID when drawing nn detections.
confidence (float, Optional) – Specify detection nn’s confidence threshold
sync (bool, Optional) – Store NN results for preview syncing (to be used with SyncedPreviewManager
- sourceChoices = ('color', 'left', 'right', 'rectifiedLeft', 'rectifiedRight', 'host')
List of available neural network inputs
- Type
- source = None
Selected neural network input
- Type
- inputSize = None
NN input size (width, height)
- Type
- openvinoVersion = None
OpenVINO version, available only if parsed from config file (see
readConfig())
- inputQueue = None
DepthAI input queue object that allows to send images from host to device (used only with
hostsource)
- outputQueue = None
DepthAI output queue object that allows to receive NN results from the device.
- buffer = {}
nn data buffer, disabled by default. Stores parsed nn data with packet sequence number as dict key
- Type
- readConfig(path)
Parses the model config file and adjusts NNetManager values accordingly. It’s advised to create a config file for every new network, as it allows to use dedicated NN nodes (for MobilenetSSD and YOLO) or use custom handler to process and display custom network results
- Parameters
path (pathlib.Path) – Path to model config file (.json)
- Raises
ValueError – If path to config file does not exist
RuntimeError – If custom handler does not contain
draworshowmethods
- createNN(pipeline, nodes, blobPath, source='color', useDepth=False, minDepth=100, maxDepth=10000, sbbScaleFactor=0.3, fullFov=True, useImageManip=True)
Creates nodes and connections in provided pipeline that will allow to run NN model and consume it’s results.
- Parameters
pipeline (depthai.Pipeline) – Pipeline instance
nodes (types.SimpleNamespace) – Object cointaining all of the nodes added to the pipeline. Available in
depthai_sdk.managers.PipelineManager.nodesblobPath (pathlib.Path) – Path to MyriadX blob. Might be useful to use together with
depthai_sdk.managers.BlobManager.getBlob()for dynamic blob compilationsource (str, Optional) – Neural network input source, one of
sourceChoicesuseDepth (bool, Optional) – If set to True, produced detections will have spatial coordinates included
minDepth (int, Optional) – Minimum depth distance in centimeters
maxDepth (int, Optional) – Maximum depth distance in centimeters
sbbScaleFactor (float, Optional) – Scale of the bounding box that will be used to calculate spatial coordinates for detection. If set to 0.3, it will scale down center-wise the bounding box to 0.3 of it’s original size and use it to calculate spatial location of the object
fullFov (bool, Optional) – If set to False, manager will include crop offset when scaling the detections. Usually should be set to True (if you don’t perform aspect ratio crop or when keepAspectRatio flag on camera/manip node is set to False
useImageManip (bool, Optional) – If set to False, manager will not create an image manip node for input image scaling - which may result in an input image being not adjusted for the NeuralNetwork node. Can be useful when we want to limit the amount of nodes running simultaneously on device
- Returns
Configured NN node that was added to the pipeline
- Return type
- Raises
RuntimeError – If source is not a valid choice or when input size has not been set.
- getLabelText(label)
Retrieves text assigned to specific label
- Parameters
label (int) – Integer representing detection label, usually returned from NN node
- Returns
Label text assigned to specific label id or label id
- Return type
- Raises
RuntimeError – If source is not a valid choice or when input size has not been set.
- parse(blocking=False)
- decode(inNn)
Decodes NN output. Performs generic handling for supported detection networks or calls custom handler methods
- Parameters
inNn (depthai.NNData) – Integer representing detection label, usually returned from NN node
- Returns
Decoded NN data
- Raises
RuntimeError – if outputFormat specified in model config file is not recognized
- draw(source, decodedData)
Draws NN results onto the frames. It’s responsible to correctly map the results onto each frame requested, including applying crop offset or preparing a correct normalization frame, then draws them with all information provided (confidence, label, spatial location, label count).
Also, it’s able to call custom nn handler method
drawto hand over drawing the results- Parameters
source (depthai_sdk.managers.PreviewManager | numpy.ndarray) –
Draw target. If supplied with a regular frame, it will draw the count on that frame
If supplied with
depthai_sdk.managers.PreviewManagerinstance, it will print the count label on all of the frames that it storesdecodedData – Detections from neural network node, usually returned from
decode()method
- createQueues(device)
Creates output queue for NeuralNetwork node and, if using
hostas asource, it will also create input queue.- Parameters
device (depthai.Device) – Running device instance
- closeQueues()
Closes output queues created by
createQueues()
- sendInputFrame(frame, seqNum=None)
Sends a frame into
inputQueueobject. Handles scaling down the frame, creating a properdepthai.ImgFrameand sending it to the queue. Be sure to usehostas asourceand callcreateQueues()prior input queue.- Parameters
frame (numpy.ndarray) – Frame to be sent to the device
seqNum (int, Optional) – Sequence number set on ImgFrame. Useful in synchronization scenarios
- Returns
scaled frame that was sent to the NN (same width/height as NN input)
- Return type
- Raises
RuntimeError – if
inputQueueisNone(unable to send the image)
- countLabel(label)
Enables object count for specific label. Label count will be printed once
draw()method is called